AXIS#.WS.CHECKV

Description

This parameter sets the velocity threshold which has to be exceeded to activate commutation monitoring.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPMClosed"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.WS.CHECKV 0x5013 0xB DINT - Velocity RW False
AXIS2.WS.CHECKV 0x5113 0xB DINT - Velocity RW False